Unable to put MCP5675K into debug mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to put MCP5675K into debug mode

ソリューションへジャンプ
2,167件の閲覧回数
danmaneu
Contributor I

Hello,

I am trying to put MCP5675K into debug mode but I am failing to do so.

I am using OpenOCD with FT2232H with custom scripting. This is based on this patch.

TRST is connected to JCOMP, SRST to chip reset (RESET_B).

I am able to see correct JTAG ID and OnCE ID.

I am trying based on AN4356 as it says:

1. Assert RESET.
2. Set the OCR[DR] and OCR[WKUP] bits.
3. Deassert RESET.
4. Verify debug mode via the DEBUG bit in the OnCE status register.
5. Clear the OCR[DR] bit while leaving OCR[WKUP] set and set OCR[FDB].

 When I set those bits, it never gets reflected in OSR (OnCE status register). I am only able to get 0x201 or 0x241 value. Never seen 0x209. This is my output:

$ ./openocd/src/openocd -f spc.cfg 
Open On-Chip Debugger 0.11.0+dev-00059-g56506d2ed (2024-01-26-00:37)
Licensed under GNU GPL v2
For bug reports, read
	http://openocd.org/doc/doxygen/bugs.html
DEPRECATED! use 'adapter speed' not 'adapter_khz'
Info : clock speed 2000 kHz
Info : JTAG tap: mcp5675.cpu tap/device found: 0x0aec101d (mfg: 0x00e (Freescale (Motorola)), part: 0xaec1, ver: 0x0)
Warn : gdb services need one or more targets defined

Sending IDCODE command

IDCODE: 0aec101d
Info : JTAG tap: mcp5675.once enabled
Info : JTAG tap: mcp5675.cpu disabled
OnCE JTAG ID = 0x07e2f01d shall be 07e2f01d
OSR = 0x0241

Enter debug mode...
asserted
ocr set
OSR = 0x0241

deasserted
OSR = 0x0201

OSR = 0x0201

OSR = 0x0201

OSR = 0x0201

OSR = 0x0201

OSR = 0x0201

My questions:

- Do you see something obvious what am I doing wrong?

- What is meant by RESET? JCOMP or chip reset?

- Is is possible the chip is in censored mode? How can I check?

0 件の賞賛
返信
1 解決策
2,137件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @danmaneu 

I shared this script based on AN4365 in the past:

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-JTAG-access-Addendum-to-application-note...

This usually helps to solve most of customers' issues.

Which TAP did you use? If your device runs in lock step mode, use ACCESS_AUX_TAP_LSM. If it is running in decoupled mode, use ACCESS_AUX_TAP_CORE_0.

RESET means chip reset, not JCOMP.

Regards,

Lukas

元の投稿で解決策を見る

2 返答(返信)
2,138件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @danmaneu 

I shared this script based on AN4365 in the past:

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-JTAG-access-Addendum-to-application-note...

This usually helps to solve most of customers' issues.

Which TAP did you use? If your device runs in lock step mode, use ACCESS_AUX_TAP_LSM. If it is running in decoupled mode, use ACCESS_AUX_TAP_CORE_0.

RESET means chip reset, not JCOMP.

Regards,

Lukas

2,132件の閲覧回数
danmaneu
Contributor I
Lukas, thank you so much! It is working now.
This was the missing piece of information:
If your device runs in lock step mode, use ACCESS_AUX_TAP_LSM.
0 件の賞賛
返信