U-Boot Bootloader for mpc5200B

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-Boot Bootloader for mpc5200B

2,874件の閲覧回数
nagaprasadvasam
Contributor III

Hi Everyone,

         Can any one help me where can i get u-boot for mpc5200b and cross compiler tool-chain  for it.if any one have any reference please share me.

Thanks&Regards,

Naga Prasad.

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,754件の閲覧回数
Pavel
NXP Employee
NXP Employee

Attachment contains u-boot source file for the Lite5200B board from LTIB Linux BSP.

Have a great day,
Pavel Chubakov

0 件の賞賛
返信

2,754件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP offers LTIB Linux BSP for the Lite5200B board:

https://www.nxp.com/lgfiles/bsps/mpc5200_lite5200b_20070203_ltib-rc4.iso

 

This BSP contains u-boot for the MPC5200B and toolchain.

This BSP was tested under Ubintu 10.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,754件の閲覧回数
nagaprasadvasam
Contributor III

Hi,

Can you share u-boot source code having configs/mpc5200_config file 

0 件の賞賛
返信