Trigger Burst Generator to trigger CFIFO

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Trigger Burst Generator to trigger CFIFO

跳至解决方案
2,013 次查看
berat24
Contributor III

Hello everyone,

I would like to consult one thing about TBG. My purpose is to trigger CFIFO with PIT periodically. I initialized MODE bits on CFCR register and ISEL registers. Also, As far as I understood, I have to initialize TBG to trigger CFIFO.

However, when I looked at the examples performed by NXP, I cannot see TBG registers.

Could you inform me what TBG is exactly?

Must I have initialize TBG for this purpose?

Sincerely.

0 项奖励
回复
1 解答
2,005 次查看
TomE
Specialist II

8.4.6 Trigger Burst Generators (TBG)

The TBG is in bypass out of reset, thus backwards compatible functionality is
provided. In this backwards compatible setting, the triggers are generated by the signals
connected to the IMUX, thus TBG is transparent to the trigger generation.

 

Tom

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,006 次查看
TomE
Specialist II

8.4.6 Trigger Burst Generators (TBG)

The TBG is in bypass out of reset, thus backwards compatible functionality is
provided. In this backwards compatible setting, the triggers are generated by the signals
connected to the IMUX, thus TBG is transparent to the trigger generation.

 

Tom

 

0 项奖励
回复