Trigger Burst Generator to trigger CFIFO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trigger Burst Generator to trigger CFIFO

Jump to solution
2,015 Views
berat24
Contributor III

Hello everyone,

I would like to consult one thing about TBG. My purpose is to trigger CFIFO with PIT periodically. I initialized MODE bits on CFCR register and ISEL registers. Also, As far as I understood, I have to initialize TBG to trigger CFIFO.

However, when I looked at the examples performed by NXP, I cannot see TBG registers.

Could you inform me what TBG is exactly?

Must I have initialize TBG for this purpose?

Sincerely.

0 Kudos
Reply
1 Solution
2,007 Views
TomE
Specialist II

8.4.6 Trigger Burst Generators (TBG)

The TBG is in bypass out of reset, thus backwards compatible functionality is
provided. In this backwards compatible setting, the triggers are generated by the signals
connected to the IMUX, thus TBG is transparent to the trigger generation.

 

Tom

 

View solution in original post

0 Kudos
Reply
1 Reply
2,008 Views
TomE
Specialist II

8.4.6 Trigger Burst Generators (TBG)

The TBG is in bypass out of reset, thus backwards compatible functionality is
provided. In this backwards compatible setting, the triggers are generated by the signals
connected to the IMUX, thus TBG is transparent to the trigger generation.

 

Tom

 

0 Kudos
Reply