The Flash memory ECC failure reporting path check

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The Flash memory ECC failure reporting path check

1,634件の閲覧回数
xiaobozheng
Contributor III

Assumption: [SM_119] The Flash memory ECC failure reporting path should be
checked to validate if detected ECC faults are correctly reported.

 

Implementation hint: The flash memory ECC fault report check is executed in
software . The test consists of software reading from the flash memory UTest area (see
"UTEST flash memory map" table in the "Memory map" chapter of the MPC5744P
Reference Manual). a set of test patterns to test the integrity of the ECC logic fault
reporting path to the MEMU and FCCU (executed at start-up, latent failure measure).

 

question:   is this means:  we can write some data into utest  region (0x00400040-0x00400060), rading it back and check the fccu or memu flag ?

   if this is not right, please tell me how can i check flash ecc failure report path,  thanks !

ラベル(1)
0 件の賞賛
返信
1 返信

1,385件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Not exactly. It is not needed to write any data to UTEST region, they are already pre-prepared there from factory (moreover UTEST region is one-time-programmable and already programmed).

I have just prepared example code here:

https://community.nxp.com/docs/DOC-333754 

0 件の賞賛
返信