TextChangeFinder Problem S32DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TextChangeFinder Problem S32DS

2,896 Views
eyupozer
Contributor III

Hi,

I have a problem with the project file or project setting on S32DS. The following error screen shows the problem but I have not found the error root yet.

How can I fix it? 

pastedImage_1.png

Thanks.

0 Kudos
Reply
3 Replies

2,855 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please clarify, which version of S32DS you use?

Have you already tried to reinstall S32DS?

Do you have installed any third party plugin in your S32DS?

Do you know, what was the trigger of this error? Have you ever been able to create a project and compile it?

Please let me know as much details as possible.

Regards,

Martin

2,855 Views
eyupozer
Contributor III

Hi,

I tried to reinstall and the problem was fixed. Thanks

S32DS version is: 

"S32 Design Studio for Power Architecture  Version: 2017.R1 Build id: 171018"

Error screen was triggered every compile, select component and debug action.

I've updated the current SDK via Help->Install New Software tool.

FYI.

0 Kudos
Reply

2,855 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

thank you for information. Maybe this could help someone other while facing this issue.

Regards,

Martin