Standby RAM Brownout Detect

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Standby RAM Brownout Detect

1,026 Views
jeromebrown_at_
Contributor I

Has  Anyone used Standby RAM Brownout Detect on the MPC5777C?

Is there any additional information on how reliable it is?

Labels (1)
0 Kudos
Reply
3 Replies

907 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

the data retention in Standby RAM is guaranteed down to 0.95V as specified in datasheet. Also the brownout detect should work as described. There are no known issues.

Are you facing any troubles with this feature?

Regards,

Lukas

0 Kudos
Reply

907 Views
jeromebrown_at_
Contributor I

Lukas,

I am trying to use it as signal to the Micro to Clear the Ram and reboot

the device.

Can it be used in this Fashion?

0 Kudos
Reply

907 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Jerome,

this flag can be used to detect if the RAM memory contains valid data after reset or power-on.

If the STND_BY_RAM_BR_DETCT is set after power-on, it says that the content of RAM has been lost (voltage fell below 0.95V on VSTBY). So, whole RAM including standby RAM must be initialized due to ECC. Then you can initialize the standby RAM, so it contains valid useful data. Then clear the STND_BY_RAM_BR_DETCT flag (first write 1 to STND_BY_RAM_BR_CLR and then write 1 to STND_BY_RAM_BR_DETCT).

After next boot (after next power-on or reset), just check the flag STND_BY_RAM_BR_DETCT. If it is 0, the content of standby RAM is valid. You do not need to initialize standby RAM, initialize only the rest of the RAM.

Regards,

Lukas

0 Kudos
Reply