[MPC5674F] ETPU library function - cam edge detection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[MPC5674F] ETPU library function - cam edge detection

1,518 Views
haksukim
Contributor I

Hello, I'm working with etpu library function (AN3769SW) and MPC5674F.

In this process, I want to detect RISING EDGE of CAM signal, so I set the parameter of CAM edge polarity to RISING_EDGE. (function: fs_etpu_app_eng_pos_init(,,,))

However, it detects only FALLING EDGE of CAM signal whatever I set the parameter.

I checked the detected CAM EDGE by a function named fs_etpu_eng_pos_get_cam_edge_angle().

How can I handle this problem?

Labels (1)
0 Kudos
Reply
1 Reply

1,357 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

In behalf of our eTPU expert:

“I can't replicate the issue. The code review (eTPU code, compiled eTPU assembly, API code) shows everything is correct. I'm short to help.

Please suggest the customer to use the new eTPU Engine Control Library instead - AN4907, AN4908.”

0 Kudos
Reply