Specific ADC channels trigger from eTPUc for MPC5777C micro

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Specific ADC channels trigger from eTPUc for MPC5777C micro

483 次查看
Amrit1
Contributor II

I want to implement a single ADC read trigger for 4 channels (ANA14 , ANA15 , ANA16_SDB0 and ANA17_SDB1 pins) within 10 micro seconds of a rising edge detection at ETPUC16 pin.
This is for a MPC5777C cobra controller
These ADCs are not differential so I don't want to configure SDADC.  

I could see from the data sheet that there is not direct trigger to do this, it can only trigger SDADC. And I would need the triggering to be fast as it has to converted and returned within 10 micro seconds.

Amrit1_0-1756452100628.png

Is there a way we can implement this? And is there any existing code which I could refer to?

 

标记 (2)
0 项奖励
回复
3 回复数

415 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Example code you may find here:

Example MPC5777C-SDADC_eTPU_triggered GHS714

https://community.nxp.com/docs/DOC-335360

However let’s talk about SDADC a bit -

Once enabled the SDADC keeps running. There is no “Single conversion mode”. This requires converted data to be continually drained by DMA or ISR. The digital nature of the SDADC means that there is a propagation delay as the data is clocked through the internal digital filters. This has to be taken into account at startup or at any channel mux change. This latency means that the SDADC is not well suited to some applications including motor control. When used in an AC sampling application it is likely that each SDADC will have to be dedicated to a particular input rather than switching the input channel.

SDADC offers higher conversion accuracy (16-bit result).

SDADC is always combined with other type of ADC, on this device it is eQADC offering advanced triggering and channel multiplexing capability (on other MPC57xx device SDADC is supplemented by SAR ADC).

So I would recommend you to use eQADC module for single triggered ADC conversions.

0 项奖励
回复

397 次查看
Amrit1
Contributor II

Understood, because I want only a single scan I am okay to use eQADC but then will I be able to trigger the ADC read when there is a rising edge on ETPUC16 pin? Because I don't see an option of ETPUC16 being a trigger for eQADC. Is my understanding correct?

标记 (2)
0 项奖励
回复

388 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

No there is no such option there. Pay attention to register SIU_ISEL4 and above:

davidtosenovjan_0-1756740688058.png

 

 

0 项奖励
回复