Source Files for RDAIRBAGPSI5 and RDAIRBAGPSI5-001 Airbag Evaluation Platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Source Files for RDAIRBAGPSI5 and RDAIRBAGPSI5-001 Airbag Evaluation Platform

2,405件の閲覧回数
radudrosescu
Contributor III

I bought two Airbag Evaluation Platform (RDAIRBAGPSI5 and RDAIRBAGPSI5-001). On the site http://www.freescale.com/arp is mentioned that kit contains Airbag System Evaluation Software (source code). RDAIRBAGPSI5 Airbag Reference Platform User Guide The only files available for the users that I found on this site are RDAIRBAGPSI5.elf, Project.abs and MiddleARD_FreeMASTER.pmp (the last for FreeMaster). I have not found codewarrior project file of ARP Graphical User Interface (GUI), source code file, MC33789.h, MMA68xx.h, MC3379.h header files, nor SPI and PSI5 communication driver source and header files.

Can someone from Freescale technical supportcenter tell me what they understand by Source Code for Airbag System Evaluation Software, how can I develop my own applications on the acquired hardware
platform using codewarrior without the abovementioned files, how to use MCAL layer?
Can I have access to the source files so I can use this platform different from
a demo software?

Thank you for your patience to read this.

Radu

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,863件の閲覧回数
ChunqiangWang
Contributor I

I am looking for the source files for RDAIRBAGPSI5. Is there any support available from NXP about this request/.

0 件の賞賛
返信

2,244件の閲覧回数
chipsoft
Contributor I

Did you found source files for RDAIRBAGPSI5? I also try to find it.

0 件の賞賛
返信