Send 32-bit SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Send 32-bit SPI

3,889 Views
CHAOWeiXu
Contributor II

hi,

I use the MPC5744P SPI module.It uses 16 bit SPI to send, but I want it to send 32 bits.I try to manually control the CS to send 32 bits.But the SCK signal will be delayed when it is sent. I want to send two 16 bits in a row.

Thanks

0 Kudos
Reply
4 Replies

3,840 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

what code do you use for this? Some delay can be caused by SW delay, also by HW (see CTAR setting).
Manual control of CS is not needed, module is able to do that, if need CS low between words use continuous selection format, check chapter 49.4.4.5 Continuous Selection Format of the RM.

BR, Petr 

0 Kudos
Reply

3,825 Views
CHAOWeiXu
Contributor II

hi,Mr,Petr 

 I use Simulink to build the model. Its name is NXP_ MBDToolbox_ MPC57xx.

I want the master to send 32-bit data to the slave, but it only supports sending 16-bit data.

When I adjust the transfer size to 32, the oscilloscope displays abnormal.When I adjust the transfer size to 16, if I send 16 bits twice in a row, there will be a delay between SCKs.In the attachment are my model and the oscilloscope image when it is sent twice in a row.

Thanks,

Tags (1)
0 Kudos
Reply

3,808 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if using MATLAB/Simulink with toolbox please ask question directly on its Community space;
https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bd-p/mbdt

BR, Petr

0 Kudos
Reply

3,805 Views
CHAOWeiXu
Contributor II

Thank you for your help.

0 Kudos
Reply