Sample LIN protocol code for MPC5777M .

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sample LIN protocol code for MPC5777M .

3,445 Views
anishchoudhary
Contributor III

I am working on MPC5777M EVB board and I want to develop LIN Protocol application on that board so any sample code of LIN is available or not in community ? and suggest me for useful document

Tags (1)
3 Replies

2,450 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you can refer to MPC5744P example posted here; https://community.nxp.com/docs/DOC-329922 

Teh LINFlex module is the same.

BR, Petr

2,450 Views
anishchoudhary
Contributor III

Hi,

In the case of loop back test mode of LIN, external 12V is required or not.

BR, Anish

0 Kudos
Reply

2,450 Views
PetrS
NXP TechSupport
NXP TechSupport

I assume for internal loopback the transceiver is not used, so it is not needed to supply it.

BR, Petr