SWT initialization with software lock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SWT initialization with software lock

1,364件の閲覧回数
antoniograu
Contributor II

Hello,

I have some strange behavior Software Watchdog Module.

I'm able to run the SWT module and it is working properly but only if SWT_CR[HLK] is set.

I do not want to use HLK because a flash operation needs more time and this bit is only cleared when RESET.

If I don't set the HLK bit, the module is not being enabled. 

Following code is working properly: When im not in debug mode, I can see how processor restarts.

/* Prepare Local 32 Bit control register

SWT_CR |= (SWT_CR_MAP0

#if APP_DEBUG
      | SWT_CR_FRZ
#endif
      | SWT_CR_HLK
   // | SWT_CR_SLK                     //Only SLK does not start the module
      | SWT_CR_WEN
);

/* Set timeout value */
numberClkTicks= 0x186A00; // 100Ms timeout
SWT.TO.R = numberClkTicks;

SWT.CR.R = SWT_CR; // update SWT control register

In the other hand, if I comment the line  SWT_CR_HLK and I uncomment the following SWT_CR_SLK.

What I'm missing here?

Thanks in advance for your help.

タグ(2)
0 件の賞賛
返信
0 返答(返信)