STAC Interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

STAC Interface

2,240 Views
ahmedabdelhalee
Contributor II

Hello,

 

Where can I find more details about STAC "Shared Time and Counter" bus interface of eTPU module of MPC5746R?

 

I can see few details in section 43.14.6.3 of the reference manual Rev 6.

 

Thanks,

Ahmed

Labels (1)
1 Reply

2,089 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

The only info about the STAC bus is given in the RM.

The STAC bus allows an eTPU to export its timebase (TCR1/TCR2) to another eTPU as well as to other peripherals such as the eMIOS.

As you mentioned the STAC is described in the chapter 43.14.6.3. See also chapter 43.7.4 and 43.7.8; the eTPUx REDCR ((eTPU_TBR_STAC_ENGx registers) have to be properly set to configure the eTPU STAC bus operation as a STAC Server/Client module. The Server ID assignment is showed in chapter 43.1.7 STAC bus.

If the STAC-bus Export/Import feature is used, the clock ratio of eTPU : eMIOS should be 1:1 or 2:1

Chapter 42.6.3 STAC Bus Client submodule describes STAC bus usage within an eMIOS module. As there are 2 engines (2 eTPU modules) you have 4 fixed time slots.

BR, Petr