SREC flashing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SREC flashing

1,402 Views
abdelrhman
Contributor III

Hi
I have a question

When I flashed the .srec file of a project or mpc5744p simulink example, the application starts only once and after resetting the kit, the application did not start. keep in mind that I flashed this file into the flash memory not into the RAM part.

Thanks.

0 Kudos
Reply
1 Reply

1,393 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Most probably your application is missing valid RCHW (reset configuration word).

Once you load program to micro via tool, it probably set IP (instruction pointer) to the start address. (Debuggers do this by default usually)

And once you reset micro, the device will start from BAM and in BAM it will look for RCHW which define your start of you application.

Please refer to reference manual:

petervlna_0-1673433257353.png

Best regards,

Peter

0 Kudos
Reply