SREC flashing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SREC flashing

1,403件の閲覧回数
abdelrhman
Contributor III

Hi
I have a question

When I flashed the .srec file of a project or mpc5744p simulink example, the application starts only once and after resetting the kit, the application did not start. keep in mind that I flashed this file into the flash memory not into the RAM part.

Thanks.

0 件の賞賛
返信
1 返信

1,394件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Most probably your application is missing valid RCHW (reset configuration word).

Once you load program to micro via tool, it probably set IP (instruction pointer) to the start address. (Debuggers do this by default usually)

And once you reset micro, the device will start from BAM and in BAM it will look for RCHW which define your start of you application.

Please refer to reference manual:

petervlna_0-1673433257353.png

Best regards,

Peter

0 件の賞賛
返信