SPI communication pullzes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI communication pullzes

ソリューションへジャンプ
3,387件の閲覧回数
annycai
Contributor I

Currently, I’m testing the SPI communicationbetween the MPC5634 (32-bit) and the MC33810.

 

I’mlooking forward you can send me the answers about the questions are listed in the following:

 

1.           How to configure the data format when write 16-bit SPI command to a 32-bit DSPI_PUSHR register of MPC5634M?

 

Example:

 

Write SPIcommand (16-bit)

 

 

Bit15                                                                                                                                bit0


Data(command)


 

 

To DSPI_PUSHR

    

         bit16                                                                                                                                        bit31

 

 


data


 

|

 

2.           Which SPI Command (on page 29 of MC33810) should send firstly when CPU need to communicate withMC33810 according to SPI bus?

 

3.           How to check SPI BUS integrity?

 

4.           What response will send back when send ‘SPI Check Command’to MC33810?

 

5.           What response will send back when send ‘Clock Calibration Command’ to MC33810?

 

6.           Which SPI Command (list in the SPI Command table) send to MC33810 can check the SPI communication bus configurewrite, andwhat will response to the CPU (MPC5634M)?

ラベル(1)
タグ(1)
1 解決策
2,960件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

This question was answered through service request system, so I'm just updating this old thread to provide the info also to other customers.

Attached are very simple projects to test the SPI communication between MC33800 and MC33810.

元の投稿で解決策を見る

1 返信
2,961件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

This question was answered through service request system, so I'm just updating this old thread to provide the info also to other customers.

Attached are very simple projects to test the SPI communication between MC33800 and MC33810.