SPI Driver for MPC5748g

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI Driver for MPC5748g

3,098件の閲覧回数
sandeepnagaraja
Contributor III

Martin Kovar

Hi Martin,

           We have a requirement of designing a SPI driver for MPC5748g, could you please share any reference SPI driver code for MPC5748g.

 

    Regards

Sandeep Nagarajan

ラベル(1)
2 返答(返信)

2,530件の閲覧回数
sandeepnagaraja
Contributor III

Hi  Sandeep martinkovarsandeepvl

Thanks for sharing, but i have few queries:(In regard to AN4830 doc)
1. i dont understand why  below functions are used, (In regard to AN4830 doc)
memory_config_160mhz();                   /* Config wait states, flash master access, etc*/
  crossbar_config();                        /* Config crossbar */


2. Under system clock configuration function:void PLL_160MHz(void) (In regard to AN4830 doc)
  PLLDIG.PLLDV.B.PREDIV  = 1;
  PLLDIG.PLLDV.B.MFD     = 16;
  PLLDIG.PLLDV.B.RFDPHI  = 1;
  PLLDIG.PLLCAL3.R = 0x09C3C000;  //MFDEN =9999

This configuratation gives me the 16kHz as the system & PLL clock,

   But we are supposed to configure for 160Mhz.

3. As per the RM of MPC5748g, the F80 & F40 is used a peripheral clocks for DSPI & SPI Modules,
   the corresponding  MC_CGM.AC0_DC4 &  MC_CGM.AC0_DC3 are used to configure for F80 & F40,
   where once i configure these two dividers, i am facing the scene where my debugger takes the flow
  to cpu idle state(error handling conditions).

It would be helpful if i get any leads regarding the issue.

      Regards

Sandeep Nagarajan

0 件の賞賛
返信

2,530件の閲覧回数
sandeepvl
Contributor III

Please have a look at this. MPC5748G : SPI ISR sample code 

It helped me. The example code for MPC5748G is basically a loop back test.