SPC5748G flexlin LIN example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPC5748G flexlin LIN example

2,495 Views
tonytony
Contributor I

I am using the S32 SDK with the SPC5748G devkit and I have setup the linflexd_uart_echo example which works but I really need to use this peripheral as a LIN peripheral, i.e. transmit header as master and receive slave response.

Does the SDK support configuration of this peripheral as linflexd_lin (as opposed to linflexd_uart)? I don't see it as a component within S32 IDE either.

Thanks

Tony

 

0 Kudos
Reply
3 Replies

2,485 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Tony,

this was already discussed here some time ago:

https://community.nxp.com/t5/S32-SDK/MPC57XX-EAR-SDK-LIN-Master-Slave-Example-Project/m-p/890681#M95...

and I'm afraid this has not been changed. There's no LIN support in the SDK for MPC5748G.

Regards,

Lukas

 

0 Kudos
Reply

2,481 Views
tonytony
Contributor I

Thanks Lukas

Can you confirm that the hardware supports LIN coms and it's just the SDK hasn't included it.  Or there is some bigger reason why the SDK team omitted such a basic peripheral demo application?

Many thanks for your support on these topics as I try get all the peripherals I need up and running.

Rgds

Tony

 

 

0 Kudos
Reply

2,440 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Tony,

I'm sorry, I didn't get notification about new message due to some system issues. Probably too late but maybe for others: yes, LIN is supported by hardware, it's just not supported by SDK for some reasons. From reference manual: "The LINFlexD supports LIN protocol version 1.3, 2.0, 2.1 , and 2.2. "

Regards,

Lukas

 

0 Kudos
Reply