SPC5741PK1 UTEST program question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPC5741PK1 UTEST program question

1,135 次查看
lishirley
Contributor II

Hi expert,

I try to program SPC5741PK1 in UTest NVM block, and refer to MPC5744P Reference Manual,

I program 4 bytes each time, some address could program successful, but some have program error.

For example, when I program 0xCC 0xCC 0xCC 0xCC in address 0x400224, it has program error, and read out data is : 0xCD 0xCC 0xCC 0xCC. and when program 0x88 0x88 0x88 0x88 in address 0x400234, it have error too, and the read out value is 0x88 0x88 0x88 0x98, as the picture shows below, the left is the read out data, the right is the write date file.Capture.PNG

I found in the RM that some address in Utest area are mapping to register, does that means it will have error when programing, would you please give me some advice for this, Thanks!

Shirley

 

0 项奖励
回复
2 回复数

1,085 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

answer can be found in the reference manual:

pastedImage_1.png

Regards,

Lukas

0 项奖励
回复

1,085 次查看
lishirley
Contributor II

Thank you very much!

BR

Shirley

0 项奖励
回复