SPC5674F Serial Bootload Code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPC5674F Serial Bootload Code

6,246件の閲覧回数
pyi285
Contributor II

I'm trying to run a bootloader through serial communication, but the program crashes in the middle of what's wrong with the code I wrote. I'm looking for someone who can explain this in detail or modify the code.
The attached file below is the code I wrote. Please refer to what the problem is.
The link is a site that was used after watching this, modifying or transforming it.
https://community.nxp.com/t5/MPC5xxx/MPC5674F-Bootload/td-p/1615404


#scp5674F #MPC5676M

0 件の賞賛
返信
11 返答(返信)

6,235件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @pyi285 

I took a quick look at your project and I can see that you are using SSD drivers from original bootloader. But it's necessary to use drivers directly for MPC5674F:

https://www.nxp.com/webapp/Download?colCode=MPC5674F_C90FL_SSD_DRV

I recommend to check section "2 MEMORY LAYOUT" in the user manual of the driver to understand the mapping. The flash is interleaved in high address space on this device, so it's little bit different here.

Regards,

Lukas

0 件の賞賛
返信

6,135件の閲覧回数
pyi285
Contributor II

I downloaded it by following the link you gave. What should I do next?

0 件の賞賛
返信

6,107件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

You should find the drivers at this path after installation:

c:\Program Files (x86)\Freescale\Standard Software C90FL Driver v1.0.4\MPC5674_5676R\

Replace the drivers in your project and see the user manual UM_C90FL_MM_SSD.pdf for details.

0 件の賞賛
返信

6,105件の閲覧回数
pyi285
Contributor II
I'm currently looking at it now. But which code is better to use, vle or book?
0 件の賞賛
返信

6,102件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Your project which you shared earlier is VLE, so you need to use VLE version of the drivers. BOOKE would not work.

0 件の賞賛
返信

6,086件の閲覧回数
pyi285
Contributor II

This is the code I made with the code link you gave. But the eraser code works, but the board receives data through serial communication (RS232) and I want to program it in the board, but it doesn't work. Can you see why?

Question
1. Serial communication is performed, but the received data is not stored in the flexi memory on the board (I sent the converted.s19 file with the Teraterm program)


2. If, after solving number 1, is there a way to jump to the desired address without resetting the board, load it from there, and run the application program (aka bootloader)?

The continued questioning may upset you, but to me it is really important.
I'm counting on you

0 件の賞賛
返信

6,063件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

1. Is Xon/Xoff flow control enabled on your host? This is a must have.

2. I do not recommend this. You would have to do complete deinitialization of everything. Reset is much more efficient.

Regards,

Lukas

0 件の賞賛
返信

6,057件の閲覧回数
pyi285
Contributor II
1. Set the current host
port: com1
Baud rate: 115200
Data: 8 bit
Parity: none
Stop: 1 bit
Flowcontrol: none

2. If you reset or turn off the power, all the contents downloaded to Flash/Ram will disappear.
0 件の賞賛
返信

5,984件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

"Flowcontrol: none" - well, as I wrote in previous post, Xon-Xoff is mandatory. It won't work without this.

0 件の賞賛
返信

5,867件の閲覧回数
pyi285
Contributor II

Could you please take a look at my code? I did everything, but the problem is AppExecute(); The bootloader does not work when I use the function. Can you tell me if there is something wrong?

0 件の賞賛
返信

6,095件の閲覧回数
pyi285
Contributor II
Thank you very much for your steady reply
0 件の賞賛
返信