SPC5607B SWT Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPC5607B SWT Problem

3,345 Views
yankuang1
Contributor III

Hi ,

I set the timeout reset time of SWT to 10s, and when I enable the interruption, SWT can normally reset after 10s timeout and F_CHECKSTOP set.

But if the interrupt is not turned on, 20s is needed before resetting. The resetting register is F_SOFT. Please help to check why this situation occurs.

0 Kudos
Reply
1 Reply

3,250 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

reference manual:

pastedImage_2.png

If the interrupt is not enabled the device will be reset after 10s

If it is enabled and not SWT in not updated in interrupt it will reset on second timeout. 20s

regards,

Peter

0 Kudos
Reply