SPC5606S code flash programmer issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPC5606S code flash programmer issue

2,086 次查看
skysword
Contributor II

I have problem of  code flash program with CW 10.7 and P&E USB multilink Universal. After flash image is downloaded to CPU and Program cannot run correctly,  But RAM image is download to ECU and Program can run correctly.

 

I wonder if there is no correct parameters configuration program download.

We can see if you can help me find a problem or there is no program to download the relevant documents.

 

 

Thanks a lot for your help!

 

The following is the configuration interface:

175843_175843.pngpastedImage_1.png

 

The contents of console  are as follows:

fl::target -lc "download"

fl::target -b 0x40000000 0xc000

fl::target -v off -l off

cmdwin::fl::device -d "MPC5606S_CODE_FLASH_VLE" -o "1Mx32x1" -a 0x0 0xfffff

cmdwin::fl::erase all

 Beginning Operation ...   

-------------------------

Chip erase not supported. Erasing sector by sector.  

Performing target initialization ...   

Reading SSCM.STATUS ...

MCU not in single chip mode.

Set interrupt vector base address at 0x40000000

init ECC SRAM 0x40000000:0xC000

Get application entry point ...

Searching for boot sectors ...

Found boot sector at 0x0000 and entry point at 0xe0.

 Downloading Flash Device Driver ...  

 Reading flash ID ...

Erasing Sector 0x00000000 to 0x00007FFF  

Erasing Sector 0x00008000 to 0x0000BFFF  

Erasing Sector 0x0000C000 to 0x0000FFFF  

Erasing Sector 0x00010000 to 0x00017FFF  

Erasing Sector 0x00018000 to 0x0001FFFF  

Erasing Sector 0x00020000 to 0x0003FFFF  

Erasing Sector 0x00040000 to 0x0005FFFF  

Erasing Sector 0x00060000 to 0x0007FFFF  

Erasing Sector 0x00080000 to 0x0009FFFF  

Erasing Sector 0x000A0000 to 0x000BFFFF  

Erasing Sector 0x000C0000 to 0x000DFFFF  

Erasing Sector 0x000E0000 to 0x000FFFFF  

 Erasing .........

 Erase Command Succeeded   

cmdwin::fl::blankcheck all

 Beginning Operation ...   

-------------------------

 Downloading Flash Utility Driver ...  

Performing Blank Check from 0x00000000 to 0x000FFFFF ...   

 Blank Checking ...

 Blank Check Succeeded   

Blank Check Completed Successfully  

cmdwin::fl::image -f "F:\\Users\\yzj\\workspace - 20160207\\MPC560xS_ADC_SW_scan\\MPC5606S_INTERNAL_FLASH\\MPC560xS_ADC_SW_scan.elf" -t "Auto Detect" -re off -oe off

cmdwin::fl::write

-------------------------

Programming file F:\Users\yzj\workspace - 20160207\MPC560xS_ADC_SW_scan\MPC5606S_INTERNAL_FLASH\MPC560xS_ADC_SW_scan.elf  

Auto-detection is successful.  

  File is of type Elf Format.  

 

 Downloading Flash Device Driver ...  

 Reading flash ID ...

Auto-detection is successful.  

  File is of type Elf Format.  

 

Downloading 0x00000008 bytes to be programmed at 0x00000000  

Executing program ....  

 Program Command Succeeded   

Downloading 0x0000028C bytes to be programmed at 0x00000020  

Executing program ....  

 Program Command Succeeded   

Downloading 0x000001A4 bytes to be programmed at 0x00001000  

Executing program ....  

 Program Command Succeeded   

Downloading 0x000003DC bytes to be programmed at 0x00002000  

Executing program ....  

 Program Command Succeeded   

Downloading 0x0000000C bytes to be programmed at 0x000023E0  

Executing program ....  

 Program Command Succeeded   

cmdwin::fl::verify

-------------------------

Verifying file F:\Users\yzj\workspace - 20160207\MPC560xS_ADC_SW_scan\MPC5606S_INTERNAL_FLASH\MPC560xS_ADC_SW_scan.elf  

Auto-detection is successful.  

  File is of type Elf Format.  

 

Auto-detection is successful.  

  File is of type Elf Format.  

 

Reading 0x00000008 bytes starting from address 0x00000000  

Reading 0x0000028C bytes starting from address 0x00000020  

Reading 0x000001A4 bytes starting from address 0x00001000  

Reading 0x000003DC bytes starting from address 0x00002000  

Reading 0x0000000C bytes starting from address 0x000023E0  

Verify Command Succeeded  

标签 (1)
0 项奖励
回复
2 回复数

1,743 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

your settings seems to be correct.

What is the behavior difference between RAM and Flash target? What does not run correctly using Flash target?

Could you please share your project? I need to check on my side.

Regards,

Martin

0 项奖励
回复

1,743 次查看
skysword
Contributor II

hello,Martin:

        

I use 1 IO port control lit a LED lamp, with RAM debugging can be lit, with FLASH download can not be lit. But the problem has been solved, found to be disconnected from burning and write, and then re power on.

Thank you very much.

Regards,

zhijian

0 项奖励
回复