SPC5605B SPI read RX problem?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPC5605B SPI read RX problem?

1,695件の閲覧回数
wuxuliang
Contributor II

 CW2.10,attatchments are project  software files.At the end of main.c , I find some SPI -read ing debug errors about breakpoint position setting.

When debuging breakpoint sets at 1st breakpoint,RX is OK,and Oscilloscope observation waveform is the correct output。

 

When debuging breakpoint sets at 2nd breakpoint,RX is error,and Oscilloscope observation waveform is the correct output。

 

I want to know if there are some errors about SPI init?

Original Attachment has been moved to: main.c.zip

Original Attachment has been moved to: Project_1(SPI)---read(遗留问题).zip

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,518件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please clarify, where did you have breakpoints placed during debugging?

Regards,

Martin

0 件の賞賛
返信