S32R274 SWT TIF Bit not set on SWT timeout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32R274 SWT TIF Bit not set on SWT timeout

ソリューションへジャンプ
3,382件の閲覧回数
lakshmikanth
Contributor III

Hi NXP, 

Does NXP supply 'FCCU' MCAL plugin for EB Tresos. I'm working on S32R274 based autosar MCAL project. And I'm unable to verify RESET action on SWT Timeout. Only 'INTERRUPT' on SWT Timeout works fine.

Is it that: Integrating 'Legacy FCCU configuration' code in to MCAL code the only solution or it can be handled in some other way?

2) Does SWT_TIF bit act as trigger to FCCU ?

Your valuable suggestions are much appreciated. 

Thanks...!

#s32r274‌ #swt‌ #fccu‌ #mcal‌ 

ラベル(1)
1 解決策
3,160件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

S32R274 MCAL is developed according to ISO26262 standard.

part of it is also Mcem driver which handles FCCU periphery.

SWT_TIF acts at a trigger for FCCU. When TIF is set it will poll a fault reporting line to FCCU.

Peter

One Tip: If you have already set TIF and the reporting line to FCCU is polled. You have no other choice then reset to clear SWT flag from FCCU NCFSx register.

元の投稿で解決策を見る

4 返答(返信)
3,161件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

S32R274 MCAL is developed according to ISO26262 standard.

part of it is also Mcem driver which handles FCCU periphery.

SWT_TIF acts at a trigger for FCCU. When TIF is set it will poll a fault reporting line to FCCU.

Peter

One Tip: If you have already set TIF and the reporting line to FCCU is polled. You have no other choice then reset to clear SWT flag from FCCU NCFSx register.

3,160件の閲覧回数
lakshmikanth
Contributor III

Hi Peter,

Thank you for the valuable information.

I'm trying it now. Will get back to you soon on the status.

Regards,

Lakshmi Kanth.

0 件の賞賛
返信
3,160件の閲覧回数
lakshmikanth
Contributor III

Hi Peter,

1) As per your suggestion I've configured "MCEM Module" to enable "SWT0_TimeOut Reset" request configuration of FCCU. I have integrated the module to my MCAL Project.

2) During initialization call I.e inside "MCEM_Init()" call, upon execution of the below instruction: (in T32_LauterBach)

             /* Clear all pending faults (W1C) */

             REG_WRITE32(FCCU_NCF_S_ADDR32(uBank),  u32ReadBack);

the "CTRL.OPS" goes to "Aborted" state. I think there is not much in 'MCEM configuration' that I may configure wrongly.

3) So, please let me know the possible reason for this "Aborted" state of FCCU.

Also, same was the case when I previously tried with the "FCCU_Init() function" from your reference code i.e 

"S32R274_Watchdog_example-S32DS" I.e after execution of the OP-1 instruction shown below and during 'while()' the "CTRL.OPS" goes to "Aborted" state.

/* enter config state - OP1 */
FCCU.CTRL.R = 0x1;

/* Verify if state change was sucessful */
while (FCCU.CTRL.B.OPS != 0x3); //operation status successful

4) So, please let me know on this issue (Currently MCAL Code is my priority than legacy) code.

Thanks in advance...! 

#fccu‌ #s32r247‌ #peter vlna‌ #SWT0TimeoutResetGeneration‌ #mcal‌

0 件の賞賛
返信
3,160件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

I am not familiar with MCAM, however I am expert in FCCU.

3. FCCU report aborted state if its configuration watchdog expires:

a) you step in debugger in while you are in FCCU CONFIG mode.

b) when you execute operation on other module then FCCU while you are in FCCU CONFIG mode

c) when you are too long in FCCU CONFIG state and your FCCU watchdog expired

d) when you ask for mode transtion to CONFIG mode with active faults in NCFSx registers.

For more details you can check my application note on FCCU configuration:

https://www.nxp.com/docs/en/application-note/AN5284.pdf?fsrch=1&sr=2&pageNum=1 

Peter