S32R FlexCan problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32R FlexCan problem

13,280 次查看
yi-linhsieh
Contributor III

Hi, 

 

I'd like to try FlexCan function on S32R EVB.

I found Example MPC5775K FlexCAN_with_interrupts_v1.1 S32DS .

I Check S32R274_IO_Signal_Description_and_Input_multiplexing_tables_Rev2,

It seems the same IO between S32R and 5775K.

So I only modified S32R timing in inital. 

 

But it not work.

I saw 5775K set  CAN_CLK at 66MHz, but S32R set CAN_CLK at 40 MHz.

Does it matter?

 

Yi-Lin

 

Kuan Hung Lin

Original Attachment has been moved to: S32R_Cubtek_77G.zip

标签 (1)
13 回复数

12,168 次查看
allenyu
Contributor II

Hi Martin,

How to set acceptance filter mask for CAN, Do you have any sample code? For example, I just want to receive a CAN ID 0x123 packet. thanks!

0 项奖励
回复

12,168 次查看
yi-linhsieh
Contributor III

Hello,

Follow your suggestion:

I runExample S32R274 FlexCAN_with_Interrupts S32DS.

I can see the TX message  output and I send single frame.

I check CAN_1.IFLAG1.R = 0 mean BUF0I isn't set.

Both of  can0 and can1 ECR = 0;

and Message buffer status are inactive. 

CAN_R.png

How to check EVB connection?

I check R156 on EVB. and it get the signal.

Are there any check points I can try?

0 项奖励
回复

12,168 次查看
martin_kovar
NXP Employee
NXP Employee

Hi,

I forgot about RX masking configured in my example. I am sending you edited example without RX masking. Please do not forget about extended ID in configured RX message buffers. Now it should work correct.

Regards,

Martin

12,168 次查看
yi-linhsieh
Contributor III

Hi Martin,

I modified the extended ID to  0,1,2.  

and  try to send data  ID with 0, 1.

But CAN_1.IFLAG1.R is still 0;

Is some thing wrong?


static void Configure_RX_MessageBuffer(void)
{

CAN_1.MB[0].CS.B.CODE = 0x0; //MB inactive
CAN_1.MB[0].CS.B.IDE = 1;
CAN_1.MB[0].ID.R = 0; //set extended ID
CAN_1.MB[0].DATA.W[1] = 0x00000000; //data1 set (optional)
CAN_1.MB[0].DATA.W[0] = 0x00000000; //data0 set (optional)
CAN_1.MB[0].CS.B.CODE = 0x4; //MB empty - ready for receive

CAN_1.MB[1].CS.B.CODE = 0x0; //MB inactive
CAN_1.MB[1].CS.B.IDE = 1;
CAN_1.MB[1].ID.R = 1; //set extended ID
CAN_1.MB[1].DATA.W[1] = 0x00000000; //data1 set (optional)
CAN_1.MB[1].DATA.W[0] = 0x00000000; //data0 set (optional)
CAN_1.MB[1].CS.B.CODE = 0x4; //MB empty - ready for receive

CAN_1.MB[2].CS.B.CODE = 0x0; //MB inactive
CAN_1.MB[2].CS.B.IDE = 1;
CAN_1.MB[2].ID.R = 2; //set extended ID
CAN_1.MB[2].DATA.W[1] = 0x00000000; //data1 set (optional)
CAN_1.MB[2].DATA.W[0] = 0x00000000; //data0 set (optional)
CAN_1.MB[2].CS.B.CODE = 0x4; //MB empty - ready for receive

}

0 项奖励
回复

12,168 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

what do you actually try to do? Do you communicate between CAN modules on EVB or you try to communicate between CAN module and PC? I saw an application in one of your post above.

The example I sent you works correct if you connect CAN modules according to the example description. If you try to communicate with PC, please check your application settings.

Without RX masking it does not matter what are the IDs in message buffer, but you must set standard or extended IDs on both sides. The code you posted above sets IDs as extended.

Regards,

Martin

12,168 次查看
yi-linhsieh
Contributor III

I try to communicate between CAN and PC. 

And yes, it's connection problem. 

It's work now.

Thanks for your help.

0 项奖励
回复

12,168 次查看
yi-linhsieh
Contributor III

It can transmit now.

But It can't trigger interrupt when receive.

Any suggestion?

0 项奖励
回复

12,168 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

at first, please check IFLAG1 register. Is BUF0I set?

If yes, please check if you have correctly installed interrupt handler (check intc_SW_mode_isr_vectors_S32R274.c file and vector 535). In MSR register, EE bit must be set. Do not forget about INTC.PSR register.

If no, you probably do not transmit message correct. In this case, check at first EVB connection. Next step is to check ECR register. Value of the register has to be zero.

Check also transmitting message buffer status. Message buffer status must be TX: Inactive after correct message transmission.

Regards,

Martin

12,168 次查看
martin_kovar
NXP Employee
NXP Employee

Hi,

there is not any difference in FlexCan bit timing, because in both cases 40MHz crystal is used. But there is a difference in signal routing on daughter cards.

I created example for S32R274, which shows, how to configure FlexCAN modules and mainly, how to connect transceivers on the NXP EVB for correct communication between modules. Please look at the example and let me know, if it works on your side.

https://community.nxp.com/docs/DOC-333702 

If you have any other questions, please feel free to write me back.

Regards,

Martin   

0 项奖励
回复

12,168 次查看
yi-linhsieh
Contributor III

Hi, 

in the header description:


 It is necessary to remove both J35 jumpers.

 Connect J35.2 to PA14 (CAN_1 TX)
 Connect J35.4 to PA15 (CAN_1 RX)

 CAN0 is connected internally to J37 (this pin is placed on daughter card)

 Connect CAN P5.2 to J37.2 (CAN_1 and CAN_0 CANL)
 Connect CAN P5.1 to J37.1 (CAN_1 and CAN_0 CANH)

I can't find P5.2 or P5.2 in  my schematic.(SPF-28921_D.pdf)

and my J35 is on MCU power connection. 

Do I need any other doc?

J35.png

0 项奖励
回复

12,160 次查看
martin_kovar
NXP Employee
NXP Employee

Hi,

I will summarize the answer to one post:

The Example will be hang at   PLL stabilization in Sysclk_Init() on my EVB.

Could you please check, if you use 40MHz crystal? If no, you have to change PLL settings.  I see I have incorrect comments in my code. Below is code with correct comments. I tested this code with 40MHz crystal and it works correct.

#define RUN0_MODE     0x4

static void Sysclk_Init(void)
{
    CGM.AC3_SC.B.SELCTL =0x01;    //connect (40MHz) XTALL to the PLL0 input

    /*Set PLL0 to 240MHz with XOSC 40MHz*/
    PLLDIG.PLL0DV.R = 0x50024030;     //predefined PLL0 divider register

    MC_ME.RUN_PC[0].R = 0xFE;        /*Enable all modes for all peripherals using
                                      ME_RUN_PC[0]*/
    MC_ME.RUN_MC[0].B.XOSCON = 1;    //Enable external oscillator
    MC_ME.RUN_MC[0].B.PLL0ON = 1;    //Enable PLL0 for RUN0 mode
    MC_ME.RUN_MC[0].B.SYSCLK = 0x2; //source PLL0 PHI for RUN0 mode

    //Mode transition to apply the PLL0 setup and set Normal mode with PLL running
    MC_ME.MCTL.R = 0x40005AF0;        //RUN0 Mode & Key
    MC_ME.MCTL.R = 0x4000A50F;        //RUN0 Mode & Key

    while(!MC_ME.GS.B.S_PLL0);      //ME_GS Wait for PLL stabilization.
    while(MC_ME.GS.B.S_MTRANS);     //Waiting for end of transaction

    /* ME_GS Check RUN0 mode has successfully been entered*/
    while(MC_ME.GS.B.S_CURRENT_MODE != RUN0_MODE);
}

In your sample, Why CAN_CLK is set to 60 MHz not 40MHz?

I set CAN Clock to 60MHz, but I do not use this clock. I use 40MHz crystal as a protocol clock instead of CAN clock. It is recommended to use crystal, because it has lower jitter and it is more accurate than CAN clock.

auxiliary clock 7 should be SPT_CLK?

Yes, auxiliary clock 7 is SPT. I took my code from MPC5775K and I did not change the comment.

Regarding you lat post, you have to look at the MPC57xx MOTHERBOARD. I am attaching it to this post.

Regards,

Martin

12,160 次查看
yi-linhsieh
Contributor III

Hi,

static void InitPeriClkGen(void)
{
...

CGM.AC2_SC.B.SELCTL = 0x2; // Select PLL0 for auxiliary clock 2
CGM.AC2_DC0.B.DIV = 3; // CAN_CLK : Enable aux clk 2 div by 4 ?(60 MHz)

CGM.AC7_SC.B.SELCTL = 0x2; // Select PLL0 for auxiliary clock 7
CGM.AC7_DC0.B.DIV = 1; // CAN_CLK : Enable aux clk 7 div by 2 ?(120 MHz)

...

}

In your sample,

Why CAN_CLK is set to 60 MHz not 40MHz?

auxiliary clock 7 should be SPT_CLK?

Yi-Lin

0 项奖励
回复

12,160 次查看
yi-linhsieh
Contributor III

Hi,

The Example will be hang at   PLL stabilization in Sysclk_Init() on my EVB.

I move the GPIO_init setting to my test code.  

But it not works.

0 项奖励
回复