S32DS initial debugging MPC5777C error reported

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS initial debugging MPC5777C error reported

1,075件の閲覧回数
zhaominyan
Contributor I

The board we designed using MPC5777C encountered the following errors in the first debugging, and the measurement reset pins were always low:

1、“The target may have entered resetescalation. Please power cycle the board.”

22fc5ae5097baabd82374e1af022e4b.png22fc5ae5097baabd82374e1af022e4b.png

2、“Warning: Device is not detected or may be censored. Please check connections or please enter password in GDB server parameters within debug configurations using the flag-uncensorpassword=n, then restart the debug session.”

97785ed2854cef5f00c597b578e86ad.png97785ed2854cef5f00c597b578e86ad.png

The following is the log during the debugging process:

Connection from "127.0.0.1" via 127.0.0.1. Connection from port "65300" to 7224
PE-ERROR: Warning. Can't read registers while part is running.
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read registers while part is running.
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
Copyright 2018 P&E Microcomputer Systems,Inc.
Command Line :D:\byd_work\S32DS\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.8.7.201906071634\win32\pegdbserver_power_console -device=MPC5777C -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=5000 -resetdelay?

CMD>RE

Initializing.

Device IDCODE is $00000377
Device ID revision is $00000001
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.

Device IDCODE is $00000377
Device ID revision is $00000001
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONC...

720a998122e98801916c1b5510099d4.png720a998122e98801916c1b5510099d4.png

dc48916275b7a2588127d884098cc1e.pngdc48916275b7a2588127d884098cc1e.png

a3928ab9839e1495130b0917ca6d647.pnga3928ab9839e1495130b0917ca6d647.png

5983400e9a569c1f0e975170dd2873c.png5983400e9a569c1f0e975170dd2873c.png

For the convenience of contact, if you have a solution, please contact my email: [email protected], please provide assistance, willingly!

タグ(2)
0 件の賞賛
返信
0 返答(返信)