S32DS SDK WKUP example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32DS SDK WKUP example

跳至解决方案
2,895 次查看
Daniel_Wax
NXP Employee
NXP Employee

Is there any particular reason that the WKUP example is setup to only run from flash?  Does anyone have an example using WKUP running out of RAM?

标签 (1)
0 项奖励
回复
1 解答
2,817 次查看
Daniel_Wax
NXP Employee
NXP Employee
0 项奖励
回复
4 回复数
2,817 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I have got feedback from SDK team.

the examples works from flash only because the wakeup procedure is simpler.

it should work from ram, if the code is put in standby ram

regards,

Peter

 

 

0 项奖励
回复
2,818 次查看
Daniel_Wax
NXP Employee
NXP Employee

Thanks Peter!

0 项奖励
回复
2,817 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Which device are you using?

regards,

Peter

0 项奖励
回复
2,817 次查看
Daniel_Wax
NXP Employee
NXP Employee

Calypso

SENT FROM PHONE

Daniel Wax | Field Applications Engineer Automotive

NXP Semiconductors

411 E Plumeria Dr

San Jose, CA 95134

office: 408-518-5533

mobile: 408-981-9220

[email protected]<mailto:[email protected]>

All types of technical support (Schematic review, layout review, software review, hardware board and software) provided

by NXP Field application team are subject to NXP's general Terms and Conditions unless superseded by a direct contract.

The information contained in this message is confidential and may be legally privileged. The message is intended solely for the addressee(s). If you are not the intended recipient, you are hereby notified that any use, dissemination, or reproduction is strictly prohibited and may be unlawful. If you are not the intended recipient, please contact the sender by return e-mail and destroy all copies of the original message.

Unless otherwise recorded in a written agreement, all sales transactions by NXP Semiconductors are subject to our general terms and conditions of commercial sale<http://www.nxp.com/about/our-terms-and-conditions-of-commercial-sale:TERMSCONDITIONSSALE?fsrch=1&sr=1&pageNum=1>.

0 项奖励
回复