S32DS For Power Archituecture

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS For Power Archituecture

1,058 Views
kmh48301
Contributor IV

Hello.

I need to use S32DS For Power Architecture IDE and M(S)PC 5775E MCU

And I need to make Library File (.a file) for it with GHS Compiler.

So i have installed and imported the GHS Compiler to S32DS For Power Architecture.

 

But I can't make Library File.

kmh48301_0-1655952402917.png

I can't see the GHS Toolchain in the selection bar.

 

when i create application project, i can see it.

kmh48301_1-1655952469038.png

 

 

Can you please give me a little hand?

I've already asked to my compiler vendor.

But he told me to ask to NXP.

 

Thanks.

Best Regards.

Phillip.

0 Kudos
Reply
0 Replies