S32 Design Studio for Power

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio for Power

Jump to solution
12,328 Views
xiaoluzxcv
Contributor I

Hello:

 

I want to know when will the S32 Design Studio for Power be released to download?

Labels (1)
1 Solution
10,546 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

In early Spetember is planed release of S32 for PPC.

Peter

View solution in original post

0 Kudos
Reply
19 Replies
10,546 Views
antoniograu
Contributor II

Any news about the release??

Regards,

Antonio

0 Kudos
Reply
10,550 Views
martin_kovar
NXP Employee
NXP Employee

Hi Antonio,

at the moment I am not able to tell you the exact date. It seems S32 could be released until the end of October. As soon as I have any information I will share it.

Regards,

Martin

0 Kudos
Reply
10,550 Views
aruneshroy
Contributor II

Is there an update on this release? Any information on what the release will contain?

0 Kudos
Reply
10,550 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

the release date has been postponed to the end of November.

Regards,

Martin

0 Kudos
Reply
10,550 Views
antoniograu
Contributor II

Hi Martin,

any news about the release???

Kind regards,
Antonio

0 Kudos
Reply
10,550 Views
enwei
NXP Employee
NXP Employee

Today is the last day of November........:smileyconfused:

0 Kudos
Reply
10,550 Views
martin_kovar
NXP Employee
NXP Employee

Hi guys,

the newest info is, that candidate release is created. To the end of this week it should be able to download S32DS from Freescale website.

Regards,

Martin

10,548 Views
martin_kovar
NXP Employee
NXP Employee

Hi guys,

I have great news for you. Since now, it is possible to download S32DS for power architecture from following link:

S32 Design Studio IDE|NXP

You can also discuss the problems at this community:

S32 Design Studio

Regards,

Martin

0 Kudos
Reply
10,548 Views
lategoodbye
Senior Contributor I

Hi Martin,

your link goes to S32 Design Studio for ARM not Power architecture.

Is this intended?

Regards

Stefan

0 Kudos
Reply
10,548 Views
martin_kovar
NXP Employee
NXP Employee

Hi Stefan,

when I click on this link S32 Design Studio IDE|NXP , it redirect me to this page:

pastedImage_1.png

Does the link redirect you to another page?


Regards,

Martin

10,544 Views
lategoodbye
Senior Contributor I

Sorry, it was my fault. I clicked on the link above which is for ARM.

0 Kudos
Reply
10,547 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

In early Spetember is planed release of S32 for PPC.

Peter

0 Kudos
Reply
10,544 Views
danielomsland
Contributor I

Hi,

Is the release in early September still on track?

Is the preview version mention in another post for internal use only?

0 Kudos
Reply
10,544 Views
martin_kovar
NXP Employee
NXP Employee

Hi Daniel,

I addressed this question yesterday and S32 should be released at the end of September or the beginning of the October.

Regards,

Martin

10,544 Views
plato
Contributor I

Hi Martin,

               now there is an upgrade available at Freescale site of S32DS but it doesn't contain any possibility to select MPC574xxP microcontroller type.

We have bought an evaluation  kit comprising KITMPC5744DBEVM, KIT33908MBEVBE, and   U-MULTILINK to evaluate this microcontroller family in order to use it in our motor control application. When it will be possible to modify and compile a project using S32DS?

Thanks and Regards

Federico

0 Kudos
Reply
10,544 Views
martin_kovar
NXP Employee
NXP Employee

Hi Federico,

I talked with my colleague about S32 for MPC this week and he has not told me the exact date yet. I will try to provide you any information as soon as possible.

Regards,

Martin

0 Kudos
Reply
10,548 Views
JChMathae
Contributor II

Yes, this would be very appreciated, to have a e200-targeted WIndows-based GCC/G++ toolchain!

Eclipse integration is not even necessary, good IDEs are freely available and we have already a decent debugger (Lauterbach TRACE32).

I am looking forward to "modern" C++ support (like C++11 in GCC3.9), and would easily do without anything else except barebone support like the classical CodeWarior __ppc_eabi_init.c initialization files.

0 Kudos
Reply
10,548 Views
thomasolenik
Contributor III

I think its great there is a plan to support the Power architecture in this new IDE. I just downloaded S32DS on October 4.  The only supported device is Kinetis KEA as of today, and its pretty bare bones.  Still, if the plan is to support the MPC5xxx MCUs, I'm excited about it.  I will check back often. I am trying to learn more about this family of MCU at my own personal expense, and a free tool chain is just what I'm looking for.

10,548 Views
michaelgoudey
NXP Employee
NXP Employee

Hi Daniel,

You should contact your Freescale Field Applications Engineer contact if you are interested in an early release version of the S32DS for PPC software.  However, you may be better off waiting for the public release at this point.

Regards,

Michael Goudey