Recent header file for MPC5748G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Recent header file for MPC5748G

3,548 Views
alexvinchev
Contributor V

Hi,

recent header files, found in AN4830, Freescale Recipes for MPC574xG - Application notes (REV 1) are 2.1.12a for mask 0N65H and 4.0.01 for mask 1N81M.

I know that there is only one newer revision for 0N65H (2.1.13).

Is there any newer revision for 1N81M? I'm asking, because supplied one is false regarding CAN1-7 definition (and maybe somewhere else), when checking versus MPC5748G - Reference Manual (REV 4) document. At least FDEN bit is not present in MCR, IMASK3 and IFLAG3 registers are missing.

Labels (1)
Tags (2)
0 Kudos
Reply
7 Replies

2,831 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Attached is latest header file ver_5.00.

EDIT: " Seems that revision 5.00 have some issues also on apps team side."

Peter

0 Kudos
Reply

2,831 Views
alexvinchev
Contributor V

Hi Peter, sorry to bother you again, but did someone tried to build with this file?

Capture.PNG

There is multiple structure (eMIOS_tag) definition at rows 14419 and 14522...

0 Kudos
Reply

2,831 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

You are right.

I wonder why author didn't tested it and put it on our official internal site.

Peter

0 Kudos
Reply

2,831 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I was speaking with apps team and they have recommended to use 4.xx version of header file.

As the 5.00 have some issue at this time.

I am not able to fix the actual header file as this must be done by application team to maintain consistency in revisions.

Peter

0 Kudos
Reply

2,831 Views
alexvinchev
Contributor V

Thanks!

This header, even with some problems, helped me in CAN FD definitions.

Greetings,

Aleksandar

0 Kudos
Reply

2,831 Views
petervlna
NXP TechSupport
NXP TechSupport

You are welcome.

Peter

0 Kudos
Reply

2,831 Views
alexvinchev
Contributor V

Thank you very much Peter!

0 Kudos
Reply