RX function problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RX function problem

2,061 次查看
金翅大鹏鸟
Contributor II

I met a problem about CAN receive problem on the platform MPC5744P;the code looks below.I can send many datas(a frame as a data) on CAN0, for example,I want to receive IDs( 0x18776260,0x18786260,0x18796260); but I can not find the mistakes. Can anyone help me to solve it ?Thank you!

标签 (1)
0 项奖励
回复
2 回复数

2,006 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

given codes do not show how the RX MB is prepared, so hard to say. Also it looks you are using individual masking registers for acceptance filters (MCR[IRMQ] set), but nowhere those registers are initialized. Note this must be done in freeze mode.   

BR, Petr

0 项奖励
回复

2,006 次查看
金翅大鹏鸟
Contributor II

Hello,

   I have set etimer0_ch0_1 in cascaded mode OK . But I can not use a single channel(such as etimer0_ch0), I can not find the problem.Can you give me a sample? 

0 项奖励
回复