RAppID Bootloader with SBC disable issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RAppID Bootloader with SBC disable issue

Jump to solution
1,996 Views
Narudol-T
Contributor III

Dear Sir,

 

I am trying to use RAppID bootloader from NXP for production code flash via CAN0

However, I found some issue with the RAppID bootloader file (MPC5744P.rbf).

 

The bootloader file does not support for SBC driver & functionality for initialization.

So, everytime I need to put SBC hardware into Debuging mode first before flashing.

 

So I want to get the project file of RAppID bootloader for MPC5744p to insert this SBC initialization.

Can you help advise/point me any direction&directory ?

 

Thank you,

Narudol T.

 

 

0 Kudos
Reply
1 Solution
1,980 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Narudol,

unfortunately the source code of rappid bootloader is considered as confidential due to some legal reasons, so it cannot be shared. We do not offer such custom update.

Regards,

Lukas

View solution in original post

0 Kudos
Reply
1 Reply
1,981 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Narudol,

unfortunately the source code of rappid bootloader is considered as confidential due to some legal reasons, so it cannot be shared. We do not offer such custom update.

Regards,

Lukas

0 Kudos
Reply