RAppID Bootloader with SBC disable issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RAppID Bootloader with SBC disable issue

ソリューションへジャンプ
2,002件の閲覧回数
Narudol-T
Contributor III

Dear Sir,

 

I am trying to use RAppID bootloader from NXP for production code flash via CAN0

However, I found some issue with the RAppID bootloader file (MPC5744P.rbf).

 

The bootloader file does not support for SBC driver & functionality for initialization.

So, everytime I need to put SBC hardware into Debuging mode first before flashing.

 

So I want to get the project file of RAppID bootloader for MPC5744p to insert this SBC initialization.

Can you help advise/point me any direction&directory ?

 

Thank you,

Narudol T.

 

 

0 件の賞賛
返信
1 解決策
1,986件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Narudol,

unfortunately the source code of rappid bootloader is considered as confidential due to some legal reasons, so it cannot be shared. We do not offer such custom update.

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,987件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Narudol,

unfortunately the source code of rappid bootloader is considered as confidential due to some legal reasons, so it cannot be shared. We do not offer such custom update.

Regards,

Lukas

0 件の賞賛
返信