Question about the ECC module in MPC5674

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about the ECC module in MPC5674

1,295 Views
youngseolee
Contributor III

Hello, NXP

 

recently, i use the MPC5674-based board, and have some questions about a ECC module in a flash memory.

 

i wanna know the ECC module of detail operation (i.e. Hamming pattern, used algorithm in modified Hamming code, etc)

 

please answer about this question.

 

thank you~

Labels (1)
0 Kudos
Reply
1 Reply

1,208 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I have mentioned used algorithm in section 2.1 of following document:

http://www.nxp.com/files/microcontrollers/doc/app_note/AN5200.pdf

It is only brief to know which algorithms are used on which MCUs. Implementation details are confidential information and it is not publicly available.

0 Kudos
Reply