Question about the ECC module in MPC5674

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about the ECC module in MPC5674

1,293件の閲覧回数
youngseolee
Contributor III

Hello, NXP

 

recently, i use the MPC5674-based board, and have some questions about a ECC module in a flash memory.

 

i wanna know the ECC module of detail operation (i.e. Hamming pattern, used algorithm in modified Hamming code, etc)

 

please answer about this question.

 

thank you~

ラベル(1)
0 件の賞賛
返信
1 返信

1,206件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I have mentioned used algorithm in section 2.1 of following document:

http://www.nxp.com/files/microcontrollers/doc/app_note/AN5200.pdf

It is only brief to know which algorithms are used on which MCUs. Implementation details are confidential information and it is not publicly available.

0 件の賞賛
返信