Question about downloading elf file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about downloading elf file

2,107 Views
qiaodeng
Contributor II

Hi,

   I am studying MPC5746R MCAL sample application. According to the document :

pastedImage_1.png

But I do not have Lauterbach.  Can I load the *elf file  to my target using GreenHills or S32 Studio? How should I do that?

Thanks,

Qiao

0 Kudos
Reply
4 Replies

1,925 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Its good to make clear some facts:

1. Compiler - Greenhills, S32DS, Windriver, etc...

2. Debugger - Lauterbach, iSystem, PEMicro,Greenhills probe, etc...

To load elf file you need a debugger which you connect to microcontroller. If you don't have Lauterbach you can use any other debugger to lead *elf file.

Peter

0 Kudos
Reply

1,925 Views
qiaodeng
Contributor II

Hi Peter,

    The debugger I use is PEMicro.  I mean is it possible to use S32 Studio or GreenHills to do the work   what  Trace32 does(import the *elf then download it to my target)

Regards,

Qiao

0 Kudos
Reply

1,925 Views
stanish
NXP Employee
NXP Employee

Hi Qiao,

you can use S32 Design Studio to program your .elf into the device since MPC5746R is supported.

See some info e.g. here:https://community.nxp.com/docs/DOC-332252 

Stan

0 Kudos
Reply

1,925 Views
qiaodeng
Contributor II

Hi Stan,

     I've followed the instruction to download the .elf  and encountered this error:

pastedImage_1.png

How could I handle this?

Regards,

Qiao

0 Kudos
Reply