Quadrature Encoder Help

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Quadrature Encoder Help

跳至解决方案
2,136 次查看
William_Klaus
Contributor II

Hello everyone.

I'm building a 100 kW traction set composed by a 3PH inverter and a PMSM, and I need to read the signals from an HS35 encoder from Bei (open colector output) for IFOC control. I'm using the MPC5775E EVB for this application, along with an interface board with my own gate drivers, sensors and all. I've seen some materials using the FTM on a LPC86x and with a S32K144, but couldn't find any using 577x microcontrollers. There's no topic in the datasheet related to it either.

Is there any documentation related to quadrature encoder reading for this microcontroller? Should I build a dedicated PCB for decoding the encoder signals?

Thanks for the help! 

0 项奖励
回复
1 解答
2,110 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

We can offer following:

Encoder is possible to do with eTPU.

https://www.nxp.com/webapp/etpu/

We even offer function which will run on MPC5775E.

Here is the older application note. I do not have personal experience with it.

https://www.nxp.com/docs/en/application-note/AN2842.pdf

Please have a look if this helps.

Best regards,

Peter

在原帖中查看解决方案

2 回复数
2,111 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

We can offer following:

Encoder is possible to do with eTPU.

https://www.nxp.com/webapp/etpu/

We even offer function which will run on MPC5775E.

Here is the older application note. I do not have personal experience with it.

https://www.nxp.com/docs/en/application-note/AN2842.pdf

Please have a look if this helps.

Best regards,

Peter

2,105 次查看
William_Klaus
Contributor II
Thank you Peter!
0 项奖励
回复