Quadrature Encoder Help

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Quadrature Encoder Help

Jump to solution
2,163 Views
William_Klaus
Contributor II

Hello everyone.

I'm building a 100 kW traction set composed by a 3PH inverter and a PMSM, and I need to read the signals from an HS35 encoder from Bei (open colector output) for IFOC control. I'm using the MPC5775E EVB for this application, along with an interface board with my own gate drivers, sensors and all. I've seen some materials using the FTM on a LPC86x and with a S32K144, but couldn't find any using 577x microcontrollers. There's no topic in the datasheet related to it either.

Is there any documentation related to quadrature encoder reading for this microcontroller? Should I build a dedicated PCB for decoding the encoder signals?

Thanks for the help! 

0 Kudos
Reply
1 Solution
2,137 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

We can offer following:

Encoder is possible to do with eTPU.

https://www.nxp.com/webapp/etpu/

We even offer function which will run on MPC5775E.

Here is the older application note. I do not have personal experience with it.

https://www.nxp.com/docs/en/application-note/AN2842.pdf

Please have a look if this helps.

Best regards,

Peter

View solution in original post

2 Replies
2,138 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

We can offer following:

Encoder is possible to do with eTPU.

https://www.nxp.com/webapp/etpu/

We even offer function which will run on MPC5775E.

Here is the older application note. I do not have personal experience with it.

https://www.nxp.com/docs/en/application-note/AN2842.pdf

Please have a look if this helps.

Best regards,

Peter

2,132 Views
William_Klaus
Contributor II
Thank you Peter!
0 Kudos
Reply