Project compiled by S32 2017.R1 is not working with booloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Project compiled by S32 2017.R1 is not working with booloader

2,013 Views
jeromeli
Contributor I

Hi,

My project that compiled in S32DS 2017.R1 is not working with my CAN bootloader. While the bootloader is fine with projects that are compiled in S32DS v1.1/v1.2. 

MCU: MPC5748G

SDK: EAR 0.8.1

Any suggestion on how to study the cause of the problem? Thanks!

3 Replies

1,832 Views
martin_kovar
NXP Employee
NXP Employee

Hello Jerome,

could you please specify, what does it mean application is not working? I need to know as much details as possible.

Just quick question, do you place anything into custom RAM section?

Regards,

Martin

1,832 Views
jeromeli
Contributor I

Hello Martin,

Thanks for the reply.

I've managed to get rid of this problem already, though I'm not quite sure about the real cause. The thing is that I use pit in the bootloader, if I disable pit before jumping to app, then it works fine. But the situation is not the same when I use S32DS v1.1/v1.2. Do you have any idea?

0 Kudos
Reply

1,832 Views
martin_kovar
NXP Employee
NXP Employee

Hello Jerome,

unfortunately, I do not have enough information, so I do not have any idea, what could be wrong.

I can recommend you some general points.

If your bootloader runs the application directly without microcontroller reset, please ensure that bootloader cleans up all resources which it used. 

Also, you did not explain the behavior. Does it mean that bootloader does not run the application at all, or application does not run correct, or...?

Please write me back as much details as possible.

Regards,

Martin