Problem while Running in stand alone without Debugger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem while Running in stand alone without Debugger

1,832件の閲覧回数
chidambaramvelu
Contributor II

Dear All,

 

I am using MPC5777M development board with Engineering Sample controller (PPC5777MMVU8A) and programmed through P&E Multilink Debugger and the device is running in standalone, but when using Mask specification qualified controller (SPC5777MMVU8) with the same debugger and same development board, the device is working while debugging and after the removal of debugger/ next Power On, the program is not working.

 

Is there any issue with debugger or in project settings..???

 

Kindly revert me as soon as possible.

ラベル(1)
2 返答(返信)

1,671件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

 

there is one difference between PPC and SPC microcontrollers. SPC microcontroller's BAM sets RUN_CFG bit in register PCTL15 to value 3. If you do not know this fact it leads to incorrect Mode Entry module settings and SIUL2 peripheral should be frozen. This does not happen with debugger, because if PEMicro debugger is connected, BAM is not executed by default.

 

Please add the following code somewhere to your Mode Entry module settings (before you do mode transition):

MC_ME.PCTL15.B.RUN_CFG = 0;

 

You described the problem generally, so I hope this helps you. If not, please write me back and describe your problem more detail.

 

Regards,

Martin

1,671件の閲覧回数
chidambaramvelu
Contributor II

Thanks Martin Kovar,

Now it's working fine in our board.

0 件の賞賛
返信