Power failed while erasing MPC5777C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power failed while erasing MPC5777C

2,899 Views
NAIDU
Contributor III

Hi,

  I am using MPC5777C controller in which while loading program(erasing) power is off after that i am unable to program the controller. previously it is working fine.following message is coming in console

verifying object file CRC....

i am using PE micro multilink universal debugger.

Please suggest some solution.

Thanks&Regards,

Naidu.

5 Replies

2,704 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

By cutting of power during programing flash you have most probably created multibit ECC errors in flash.

Did you tried to erase whole micro flash?

Can you see that flash is correctly erased before you begin code loading?

Peter

2,704 Views
NAIDU
Contributor III

Dear Peter,

please suggest how can i erase the 5777C controller flash using S32DS software with out programming .

Please suggest at the earliest as we have stucked up because of this issue.

Thanks&Regards,

Naidu

0 Kudos
Reply

2,704 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

unfortunately I am not working with PE and S32DS.

I am always using Lauterbach and GHS. I can guide you here if you want.

According to my colleague only erase is not supported in PE. However there can be used workaround by generating empty S records and loading it as PE erase whole micro on programming.

Peter

2,704 Views
NAIDU
Contributor III

Hi Peter,

Thank you for your response.

So if I understood you correctly, you have lost power during erase.--------yes

Were you erasing whole internal flash of micro?----yes

Do you see permanent reset on reset pin?----no

Today i captured console log in S32DS and is attached for your reference.

Following are some more observations

1.verifying object file CRC.... after this message it is taking more time

2.After that things are happening as per attached log.

Console Log.jpg

Thanks&Regards,

Naidu.

0 Kudos
Reply

2,704 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

So if I understood you correctly, you have lost power during erase.

Were you erasing whole internal flash of micro?

Do you see permanent reset on reset pin?

Peter