Possibility of using lin master node to receive lin frames from other master nodes(MPC%/$(G)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Possibility of using lin master node to receive lin frames from other master nodes(MPC%/$(G)

1,038 Views
ZD-Zhengkun
Contributor II

Hi,

I am using MPC5748g to receive lin frames, but according to the reference manual, only LINFlexD0 can be configured as the slave node, the others can only be configured as lin master. Thus, I have a question, is it possible to use LINFlexD1~17 as the master node and receive the lin frames from the other master nodes? Since they can receive the frames from slave nodes that contain only data without a header, is there a solution to extract the data from frames(wither header) from other master nodes?

BR,

Zhengkun Li

Tags (3)
0 Kudos
Reply
1 Reply

1,029 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I am not completely sure if i understand what you want to achieve. Do you want to perform the test as shown in the following example code?

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5748G-LINFlex-LIN-Master-Slave-test-G...

 

 

0 Kudos
Reply