PE Micro Multilink Universal loading code issue.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PE Micro Multilink Universal loading code issue.

1,083件の閲覧回数
Vamsi_Tellapandla
Contributor I

I am using PE Micro Multilink Universal(Part# USB-ML-UNIVERSAL) for code loading with MPC5554 controller. When i am trying to load the code using E Sys flasher 1.22 it is getting "Could not establish communication with device!" message. Kindly suggest troubleshooting methods for this issue.

d595f5e7-74d8-484a-83dc-b026f3b0a664.jpgd595f5e7-74d8-484a-83dc-b026f3b0a664.jpg

IMG-20240828-WA0003.jpgIMG-20240828-WA0003.jpg

IMG_20240828_121109.jpgIMG_20240828_121109.jpg

0 件の賞賛
返信
1 返信

1,068件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

eSYS flasher is no longer supported by NXP. There are currently no plans for its update.

Possible alternatives is following:

PeMicro has a tool called PROGPPCNEXUS. It is flash programmer and with this you can do all these operations. In the attached screenshot you can see how to upload MCU memory content into s19 file (S-record) and with this tool you can also erase the chip and program it.

PeMicro offers their own debugger (called 64K Starter Edition of P&E's PKGPPCNEXUS. Trial version is free (it is needed to be registered and logged in), programmer is part of the package:

http://www.pemicro.com/downloads/download_file.cfm?download_id=194

 

For further detail I would recommend to contact PeMicro support:

https://www.pemicro.com/support/index.cfm

 

See http://www.pemicro.com/

0 件の賞賛
返信