OpenSDA S32R274

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,763件の閲覧回数
longfeiwang
Contributor III

Does opensda support s32r274?If I do my own opensda,Does the USB bootloader in the chip come with itself or need to be obtained from other channels?

0 件の賞賛
返信
1 解決策
1,739件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

AFAIK OpenSDA does not support S32R274. Anyway to be 100% sure please check it with Pemicro support (OpenSDA release notes are not very specific about supported derivatives)

Regarding OpenSDA bootloader/application - Pemicro distributes it in a single package along with other OpenSDA firmwares:

http://www.pemicro.com/opensda/

The bootloader/application is distributed as .sda file and could be programmed e.g. by CycloneMAX programmer.

For more information about OpenSDA I'd suggest you to contact Pemicro Support.

Hope it helps.

Stan

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,740件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

AFAIK OpenSDA does not support S32R274. Anyway to be 100% sure please check it with Pemicro support (OpenSDA release notes are not very specific about supported derivatives)

Regarding OpenSDA bootloader/application - Pemicro distributes it in a single package along with other OpenSDA firmwares:

http://www.pemicro.com/opensda/

The bootloader/application is distributed as .sda file and could be programmed e.g. by CycloneMAX programmer.

For more information about OpenSDA I'd suggest you to contact Pemicro Support.

Hope it helps.

Stan

 

0 件の賞賛
返信