On-platform versus Off platform peripherals

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

On-platform versus Off platform peripherals

Jump to solution
2,239 Views
yaort_amoureux
Contributor II

What is mean by On-platform and Off platform peripherals in MPC5643L reference manual ?

Tags (1)
1 Solution
2,131 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

let‘s define what the platform is - it is the core and surrounding peripherals tightly tied to the core (thus ON platform modules are INTC, XBAR, or PBRIDGE itself...) making such independent unit. On the safety devices where two cores can run in lockstep mode (MPC5643L or MPC5675K) such unit is also called sphere of replication.
OFF platform peripheral are mostly communication modules, ADCs and so on, thus these are not system modules tightly tied to the core (on safety device are not being replicated).

Regards,
Lukas

View solution in original post

1 Reply
2,132 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

let‘s define what the platform is - it is the core and surrounding peripherals tightly tied to the core (thus ON platform modules are INTC, XBAR, or PBRIDGE itself...) making such independent unit. On the safety devices where two cores can run in lockstep mode (MPC5643L or MPC5675K) such unit is also called sphere of replication.
OFF platform peripheral are mostly communication modules, ADCs and so on, thus these are not system modules tightly tied to the core (on safety device are not being replicated).

Regards,
Lukas