On-platform versus Off platform peripherals

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

On-platform versus Off platform peripherals

ソリューションへジャンプ
2,233件の閲覧回数
yaort_amoureux
Contributor II

What is mean by On-platform and Off platform peripherals in MPC5643L reference manual ?

タグ(1)
1 解決策
2,125件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

let‘s define what the platform is - it is the core and surrounding peripherals tightly tied to the core (thus ON platform modules are INTC, XBAR, or PBRIDGE itself...) making such independent unit. On the safety devices where two cores can run in lockstep mode (MPC5643L or MPC5675K) such unit is also called sphere of replication.
OFF platform peripheral are mostly communication modules, ADCs and so on, thus these are not system modules tightly tied to the core (on safety device are not being replicated).

Regards,
Lukas

元の投稿で解決策を見る

1 返信
2,126件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

let‘s define what the platform is - it is the core and surrounding peripherals tightly tied to the core (thus ON platform modules are INTC, XBAR, or PBRIDGE itself...) making such independent unit. On the safety devices where two cores can run in lockstep mode (MPC5643L or MPC5675K) such unit is also called sphere of replication.
OFF platform peripheral are mostly communication modules, ADCs and so on, thus these are not system modules tightly tied to the core (on safety device are not being replicated).

Regards,
Lukas