Need sample code MPC5777M Fast Ethernet Controller to communicate TJA1100 NXP PHY

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need sample code MPC5777M Fast Ethernet Controller to communicate TJA1100 NXP PHY

2,705 Views
chidambaramvelu
Contributor II

Hi all,

 We are using MPC5777M Controller in our project. I have to communicate with Ethernet Controller with TJA1100 (OPEN Alliance Broad R-Reach PHY for Automotive Ethernet). I need sample code, Application Note  for Fast Ethernet controller and guidelines for that.

Labels (1)
0 Kudos
Reply
1 Reply

2,052 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

There is a app note AN4577 : Using the Fast Ethernet Controller on the Qorivva MPC564xB/C (http://cache.freescale.com/files/32bit/doc/app_note/AN4577.pdf) with the software example. The FEC module is the same.

 

Attached is the AN4577 example 1 ported to the MPC5777M EVB board. You can test it directly if upi have the EVB.

There is DP83848c PHY, but I think it will be very similar.

 

Hope it helps.

BR, Petr

0 Kudos
Reply