NPC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,247件の閲覧回数
zhhq123
Contributor II

Hi,
I want to Use MSEO1 as SPI_SI, EVTO as SPI_SO and MSEO0 as SPI_SCLK,Is there any Example code or advice ?
Best Regards.

0 件の賞賛
返信
1 解決策
3,215件の閲覧回数
zhhq123
Contributor II

I misunderstood the use of these PINs.

I used SIU to cofig these PINs to work as GPIO.

I used GPIO to stimulate SPI.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,221件の閲覧回数
juama
Contributor I

Also let me know when you found, the solution for that!

thanks

0 件の賞賛
返信
3,216件の閲覧回数
zhhq123
Contributor II

I misunderstood the use of these PINs.

I used SIU to cofig these PINs to work as GPIO.

I used GPIO to stimulate SPI.

0 件の賞賛
返信
3,235件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

it's good to mention which device you use...

Regards,

Lukas

 

0 件の賞賛
返信
3,223件の閲覧回数
zhhq123
Contributor II

MPC5634

0 件の賞賛
返信