NPC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
3,245 Views
zhhq123
Contributor II

Hi,
I want to Use MSEO1 as SPI_SI, EVTO as SPI_SO and MSEO0 as SPI_SCLK,Is there any Example code or advice ?
Best Regards.

0 Kudos
Reply
1 Solution
3,213 Views
zhhq123
Contributor II

I misunderstood the use of these PINs.

I used SIU to cofig these PINs to work as GPIO.

I used GPIO to stimulate SPI.

View solution in original post

0 Kudos
Reply
4 Replies
3,219 Views
juama
Contributor I

Also let me know when you found, the solution for that!

thanks

0 Kudos
Reply
3,214 Views
zhhq123
Contributor II

I misunderstood the use of these PINs.

I used SIU to cofig these PINs to work as GPIO.

I used GPIO to stimulate SPI.

0 Kudos
Reply
3,233 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

it's good to mention which device you use...

Regards,

Lukas

 

0 Kudos
Reply
3,221 Views
zhhq123
Contributor II

MPC5634

0 Kudos
Reply